Other Parts Discussed in Thread: PCM1808, TAS5086, TAS5162, DIR9001, TAS5162DKD6EVM, PLL1705
Hello!
a year ago I designed a class-D amplifier based on the TAS5162, pcm1808 and TAS5086. During the year, was made a few hundred samples intended to be sold to radio amateurs. Most devices are functioning properly and not cause any complaints from consumers. But some instances do not work properly.
Baseline data: Fpwm = 384kHz, PVDD = 38 V (stabilized), GVDD = VDD = 12 V, BTL mode, RL = 4Ohm, Roc = 22 kOhm. Circuit of the TAS5162
typical (as in Figure 15. Typical Non-Differential (1N) BTL Application With AD Modulation Filters).
The source of the signal typically used line-out computer sound card, headphone out of notebook.
Questions about the TAS5162:
in some cases, users complain about the failure of these chips in the long run the amplifier (more than 30min). First TAS5162 overheats and goes into protection mode, and then closes the power PVDD to GND, GND_x. Then comes the smoke and body chip breaks.
Rarely TAS5162 similarly fails at power on.
1. For whatever reason, may fail built-in protection TAS5162? Were there cases of unjustified failure of these chips in the past?
2. Is it possible failure of the chip, if heat sink is not grounded?
3. Does the quality of Low-Pass-Filter on the safety of the chip?
4. Why increase the supply voltage over 37V (Rl = 4Ohm - resistor) causes modulation of the output signal from the noise? This triggered a primary protection OCP?

Question about the TAS5086:
Sometimes there is a click when connecting / disconnecting the input from pcm1808. Then the sound just disappears. No reset or hardware enable / disable (pins PDN, RST) TAS5086 does not return it to normal operation. Only after the power cycling circuit begins to operate normally. The same problem sometimes happens in my other amplifier on the basis of TAS5504
schematic is here:
http://www.masterkit.ru/images/set_dop/bm2073_2.gif
http://www.masterkit.ru/main/scheme.php?num=1275
I hope for your help, thank you!