This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1861: differential input - missing n or p channel doesn't make a difference

Expert 1105 points

Part Number: PCM1861

Hello,

A friend suggested using the single ended measurement option of PCM1861 along with differential mode.

So first measure p and n channels seperately in single ended mode

then measure it in differential mode.

if all 3 measurements are okey then we conclude the signal is fine

what do you think?

  • Hi, Rifo,

    This approach might be used, as this analysis will dictate if all the connections to the differential input are fine. It will be a matter of selecting the device inputs used for each test by updating MD2, MD5 and MD6 configuration pins.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer