This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like you to confirm whether following description is correct or not.
* 1: Beep generator is enabled (self-clearing based on beep duration).
According to confirmation w/ CodecControl and DAC3101 EVM, when I write "1" to Add 0x47[7], I confirmed beep sound by using HP but this bitfield is NOT cleared.
So, I would like you to confirm how user can observe self-clearing in this bitfield.
Could you please confirm ?
Best regards,
Hello Ivan-san,
Thank you for your reply.
>Did you read this bit after the beep sound ended?
Yes, I performed "Refresh" from "Register Inspector" on CodecControl.
Could you please confirm whether statement is correct or not ?
I only set following registers after power on by using CodecControl.
1. Set 0x19 to Add 0x3C
2. Set 0x80 to Add 0x47
I confirmed beep sound from HP out.
Best regards,
Hello Ivan-san,
Thank you for your confirmation.
If you have any update, could you please let me know ?
Best Regards,
Hello Ivan-san,
Could you please tell me your status ?
Because, I need to inform current status to customer tomorrow.
BR,
Hello Ivan-san,
Thank you for your confirmation.
I understood that there is no issue w/ the device itself.
>My customer observe similar issue on customer's software condition, so if you locate root cause, it will become help.
However, as I described above, customer have similar issue on their system.
They are referring to following driver information.
www.ti.com/.../tlv320aic31xxsw-linux
e2e.ti.com/.../601636
It seems that you said that this issue is NOT related to device driver, related to Application layer.
Is my understanding correct ?
If no, and this is related to device driver, could you please point out source code which have problem ?
Best Regards,
Hello Ivan-san,
Thank you for your reply.
I informed that this issue is related to code of App layer not device driver to customer.
If they have additional question, I will post it to this thread.
Please keep open to confirm their feedback.
Best Regards,