Other Parts Discussed in Thread: PCM1803
Tool/software: TI C/C++ Compiler
Hi, Mr. Diego,
We got 2 questions about PCM1863
1. For the single end input connection, like the example design in TIDA-01470, when the VINL1/R1 connecting to the ADC1/2 , must I connect the VINL2/R2 to GND, or just left it float ? If so , it is just like the differential diagram.
2. For the SNR in D/S page 12, it is about 110db in typical but 97db in MIN(SE will lower for 4db), so 13db variant. Comparing to the PCM1803, it is about 103db in typical and 100db in MIN, so just 3db variant. Whcih one is the winner when more concern about the SNR or dynanmic range?
Best Regards,
James J.