This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3131D2: TPA3131 power limit and cap decoupling remove

Part Number: TPA3131D2


Hello,

1. Customer tested the output power of a 16Ohm speaker under 0dBFS, which is 2.8W and 26% THD.  Output power of Table 3 is tested when input level adjusted for 10%, does it have larger output power under 0dBFS input? What is the relationship between power limit and THD?

For PVCC power decouping above, can customer remover one set of cap and only use one set of caps to supply 13,14,27,28 pins?