This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Wayne,
TPA3131 can support 12.5W @8ohm, please refer Figure 13 in datasheet.
I think there is typo. It should be: RL = 8 Ω, f = 1 kHz, PO = 0.1W to 20 W (TPA3132D2)
Regards,
Derek