This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
I would like to use one tpa6120 to get balence output voltage shown in the pic attched. I am calculating the output current like this (assume output resistance =0) : 20v/32= 0.625A. So the tpa6120 will output 0.625A ? and what is the relation bettwen 0.625A and 10v output voltage (U=I*R) ?
I found some product using this balance circuit, so I would like to design a first version directly,but it is better to have a estimattion of one chip power current . I am not sure if a 700mA margin is enough for one chip.
Hi , that will be great helpful .
The detail specifics is : +-10v power supply for tpa6120, consider the mini load 16o, and the input balance signal is acturely +-8.5v pp because of the PGA2130' s limit . there are two tpa6120 in my design, but we can take one chip for test . (the whole system include 8 opa627, one ak4497, two PGA2130, and two TPA6120. all work in +-10v power, except ak4497 on 5v) I would like use two +- 1.5 A ldo power supply.
Hi Liang,
Below are a couple tables with current values, please note that the current value in the table is the addition of both (positive and negative) supplies. Based on this I think your 700mA is a good current range for 1 unit.
16Ω | |
mA | |
Idle | 38 |
1kHz @ 1%THD+N | 550 |
1kHz @ 10%THD+N | 628 |
32Ω | |
mA | |
Idle | 38 |
1kHz @ 1%THD+N | 400 |
1kHz @ 10%THD+N | 450 |
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Thanks a lot !
This is great helpful, and also I think this can be add to the datasheet as a common use . And one question , the 10% THD+N is too high for hifi use, so do you record the input pp voltage when the THD+N is 1% ?