This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It can be seen from the data manual that the typical value of CMRR of PCM1863 is 56dB. What is the maximum and minimum value of CMRR? We need to assess the worst in our design. In addition, how did you test this CMRR? Are there any related technical documents?
Hi Jace,
I am not sure if we have min/max value for CMRR as part of the characterization data for PCM1863. I'll look into this and see if we can support the request.
Best regards,
Ravi