This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3110D2: Is the design OK about SD# and FAULT# ?

Part Number: TPA3110D2


Dears:

Could you kindly help to check the schematic about TPA3110D2?

041111582815_16.pdf

And especially about the below design:

1. Is the design OK about SD# and FAULT# ?

2. How to set the parameters about GAIN0 and GAIN1 when the input Level is 2-3Vrms?

Pls. kindly help to give some advice.

  • Hi Luck,

    I am looking into this. Please also share basic spec with me, like PVDD, BTL?, Load=?ohm, expected maximum output power etc.


    Regards,
    Alix Wan.
  • Hi Alix:
    Pls. kindly refer the below information:
    1. PVDD
    Luck: Do you mean PVCC? PVCC is 12V.
    2.BTL:
    Luck: Using BTL output.
    3. Load=?ohm
    Luck: Every channel's load is 8 ohm, and power consumption is 5W.
    4. There are 2 channels and connect 2 Loudspeaker.
    Pls. kindly help to give some advice.
  • Hello,

    Please refer to the schematic in UG.

    SD circuit does not look good on my side. Circuit below is for your reference (you need to check based on your design)

    As to the gain setting, please refer to the datasheet. If input is too larger, you can use two 1k resistor to decrease its range. 

    Regards,

    Alix Wan.

  • Hi Alix Wan:
    Many thanks for your suggestions.
    And there are other issues about the design.
    1. Need we add ESD to protect if the loudspeaker is out?
    2. Need we choose DCDC or LDO to power supply for TPA3110D2?
  • Hello,

    Both the two questions are out of my recommendation. I would recommend to consult in power forum.
    But on my side, ESD may be needed and DCDC is more suitable here.

    Regards,
    Alix Wan.