This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: MASTER SLAVE configuration for 3 devices (TPA3255)

Part Number: TPA3255


RELATED QUESTION.  MASTER/SLAVE mode.  (3 x 3255)

I've had a look at the information in  http://www.ti.com/lit/an/slaa787/slaa787.pdf

but cannot quite work  out how to connect my 3 devices as Master and 2 slaves.
Can I simply connect the OSC-IOM of each device together? and also the OSC-IOP's to each other?
The attached image shows that in a 5 device system, sometimes the OSC IOM is connected to the OSC-IOP and 
in other devices it goes to the OSC-IOM.  
(of course also setting the master freq with the resistor)
Regards
Julian