This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM3002: PCM3002

Part Number: PCM3002
Other Parts Discussed in Thread: TLV320AIC3204, TLV320AIC3104

HI

i use PCM3002 to test audio

1: the test block is showed in the below

all power input pin is 3.3V

But Vref1 =3.3V 

Vref2= 0V 

is this correct? 

2:  i also give signal to PCM 3002 

1KHz sine wave ==> to Vin 

1.SystemCLK=4.096MHz
2.LRCIN=8KHz
3.BCKIN=256Khz

but No Dout ?

what's wrong in this operation