This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIT4096: DIT4096 sequence quetsion

Part Number: DIT4096

HI Team

          Does DIT4096 have any sequence request? for Power / Control / I2S ?

  • There is not a specified power-supply sequence for the DIT4096 but make sure you don't violate any of the maximum ratings in the datasheet.

    Datasheet Page 6 Section "Reset and Power-Down Operation" describes the mandatory reset sequence that must be used. I've copied the information below.

    The DIT4096 includes a reset input, RST (pin 15), which is
    used to force a reset sequence. When the DIT4096 is first
    powered up, the user must assert RST low, in order to start
    the reset sequence. The RST input must be low for a minimum
    of 500ns. The RST input is then forced high to enable
    normal operation. For software mode, the reset sequence will
    force all internal registers to their default settings. In addition,
    the reset sequence will force all channel status bits to 0 in
    Software mode.
    While the RST input is low, the transmitter outputs,
    TX– (pin 17) and TX+ (pin 18), are forced to ground.
    Upon setting RST high, the TX– and TX+ outputs will remain
    low until the rising edge of the SYNC clock is detected at
    pin 12. Once this occurs, the TX– and TX+ outputs will
    become active and be driven by the output of the AES-3
    encoder.
    In Software mode, the DIT4096 also includes software reset
    and power-down bits, located in control register 02H. The
    software reset bit, RST, and the software power-down bit,
    PDN, are both active high.