TPA3255 should be fully controllable with a 2.1Vrms DAC - but unfortunately it does not do this in BTL/PBTL mode.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPA3255 should be fully controllable with a 2.1Vrms DAC - but unfortunately it does not do this in BTL/PBTL mode.
Hi,
Could you share a little bit more detail? Thanks!
Looks like the TPA3255 only have 21.5dB gain. 2Vrms input would be amplified to ~24Vrms, while on 4Ohm loading, 24Vrms can only deliver 24^2/4=144W.
Did I make anything wrong?
Regards,
Hao
Hi Hao,
no but I would except that if the datasheet outlines 2Vrms DAC compatibility that this is valid for all modes not only Single-Ended and that you can reach maximum power output in all modes with a 2Vrms DAC.
Hence I expected that TPS3255 changes it's internal gain depending on the selected mode to maintain compatibility with a 2Vrms DAC.
Regards,
Sebastian