Other Parts Discussed in Thread: , TAS2563, TAS2562
Hello, TI team,
we have almost finished sound adjustments with the TAS2557EVM for our amplifier project now and
will start system integration now.
The job is to transfer all the configuration data, coefficients plus the encrypted DSP code via I2C to the TAS2557. That is understood.
1. I cannot find header files amongst the generated data. Is the header generation still nonfunctional?
2. If so, is there an external tool available to generate a proper header file?
3. PPC3 is generating a vast amount of files. Is there any documentation, what all these files are used for?
4. Where do i find the mentioned 'encrypted DSP code' and how to transfer it to the TAS2557?
Kind regards
Andreas Paulin