I'm having the damnedest time trying to get a TLV320ADC3140 to transmit I2S on a prototype I was given.
I initially tried to make it a slave but the interrupts never cleared once I powered things up, and while things were running I got no data over SDOUT, and while ASI_STS showed 0x44 most of the time, it often showed 0xf4.
Initially I was using the internal clock (samd21g18) to run a BCLK at 3.07Mhz, and 64 FS ratio, but the clocks didn't seem good enough, and got ASI_STS showing 0x44, with a lot of 0xf4, and 0x40. So I managed to hack together an XIN using a 12Mhz clock signal from another board with a 12Mhz crystal, and output 3.00Mhz BCLK and 64 FS ratio. That looked better, but I still got the occasional ASI_STS 0xf4.
Now, I'm attempting to run run the 12Mhz clock straight to GPIO1, for the master clock. If I remove the clock, I get a FS square at 7.62khz, and BCLK square at 488.1khz (using the scope's counter), equal time HI and LOW. If I add the clock (11.9997Mhz). Still no SDOUT, but FS only stays LOW for 6us for every ~94us period, and what's really goofy is that it almost looks like I'm getting data on BCLK. Meanwhile the interrupts are all over the place, as are ASI_STATUS. For a while, I thought I might have my header pins mislabeled, but I traced things back to pin 22 on the chip, and
Now, I have every reason to think this prototype is a problem in general, for all I know, there's a short on one of the ADC pins. I've ordered the 3140 dev board, and am hoping that that helps eliminate some of the issues I'm seeing. But I'm just not sure if I'm just doing something stupid in the configuration.
I'd appreciate any clues, or help.
gpio_set_pin_level(ADC_RESET, false);
delay_ms(300); //wait for ADC to hardware shutdown
gpio_set_pin_level(ADC_RESET, true);
delay_ms(50);
ADCwrite[0] = 0x02;
ADCwrite[1] = 0x81;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //wake up
delay_ms(20);
ADCwrite[0] = 0x07;
ADCwrite[1] = 0x70;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //ASI_CFG0 i2s, 32 bits, default fsync_pol, default bclk_pol, default tx_edge, tx_fill 0s
ADCwrite[0] = 0x13;
ADCwrite[1] = 0x80;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //MST_CFG0, master mode, 48k, mclk 12Mhz
ADCwrite[0] = 0x14;
ADCwrite[1] = 0x44;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //MST_CFG1, 48k, 64 fs_bclk_ratio
ADCwrite[0] = 0x16;
ADCwrite[1] = 0x88;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //CLK_CFG, MCLK audio root sourse, MCLK freq specified, MCLK to FS ratio 256
ADCwrite[0] = 0x21;
ADCwrite[1] = 0xa0;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //GPIO_CFG0, GPIO as MCLK input
ADCwrite[0] = 0x73;
ADCwrite[1] = 0xc0;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //input channels 1, 2
ADCwrite[0] = 0x74;
ADCwrite[1] = 0xc0;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //output channels 1, 2
printf("written: %d\n", written_count);
ADCwrite[0] = 0x36; //interrupt register
ADCread[0] = 0xff;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 1);
read_count = io_read(I2C_0_io, (uint8_t *)ADCread, 1);
printf("read: %d\n", read_count);
printf("interrupt: %x\n", ADCread[0]);
ADCwrite[0] = 0x36; //interrupt register
ADCread[0] = 0xff;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 1);
read_count = io_read(I2C_0_io, (uint8_t *)ADCread, 1);
printf("read: %d\n", read_count);
printf("interrupt: %x\n", ADCread[0]);
ADCwrite[0] = 0x15; //ASI_STS
ADCread[0] = 0x00;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 1);
read_count = io_read(I2C_0_io, (uint8_t *)ADCread, 1);
printf("\nread: %d\n", read_count);
printf("ASI_STS: %x\n", ADCread[0]);
ADCwrite[0] = 0x75;
ADCwrite[1] = 0xe0;
written_count = io_write(I2C_0_io, (uint8_t *)ADCwrite, 2); //power up adc, micbias, pll