Is there a simple way in which I can create an180 degree out of phase constructive interference sine-wave from one channel of my sound card to an accuracy of at least 0.1Hz, please?
Ivan Salazar kindly suggested that I use Audacity Software but regrettably it appears only to be accurate to 1Hz.
The software that I am using from 'onlinetonegenerator' has the accuracy but it does not appear to have the ablilty to create an out of phase secondary sine-wave.
Presently my sound-card is generating typically just over a 7 volt ac signal to each phase of the stereo output, and I need to achieve the output of both left and right outputs phases combined into a single mono signal. Hence why Ivan kindly suggested that I create a second out-of-phase signal from say the right-hand phase.
Your kind help would be greatly appreciated, please?
Thank you so much.
Christopher J James