This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. Team
I'm struggling to configure TLV320ADC3140 as Audio Bus Master.
And I would like to use this functional mode. (Auto Clock Generation with Internal PLL enabled)
In case of my board, 24.576MHz OSC4 is connected to GPIO1 for MCLK
And IN1P_GPI1 will be used for D-MIC data and INIP_GPO1 is going to be used for D-MIC clock.
Anyway, when I just check BCLK/FSYNC/INIP_GPO1 for D-MIC clock based on 24.576MHz MCLK, I can't see any signal coming out.
Could you let me know what I am missing to configure TLV320ADC3140 as Audio Bus Master?
Here is my register value.
===================================================
root@euto-v9:~# i2cdump -f -y 7 0x4c
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 00 00 81 00 00 05 00 70 00 00 00 00 01 02 03 04 ..?..?.p....????
10: 05 06 07 80 48 ff 10 10 04 20 02 08 00 00 02 40 ????H.??? ??..?@
20: 00 a0 40 40 00 00 00 00 00 00 00 44 00 00 00 00 .?@@.......D....
30: 00 00 00 ff 00 00 00 00 80 00 00 00 00 00 c9 80 ........?.....??
40: 00 00 00 c9 80 00 00 00 c9 80 00 00 00 c9 80 00 ...??...??...??.
50: 00 00 c9 80 00 00 00 c9 80 00 00 00 c9 80 00 00 ..??...??...??..
60: 00 c9 80 00 00 00 00 00 00 00 00 01 40 7b 00 00 .??........?@{..
70: e7 00 00 00 00 00 00 c0 00 00 ff 00 ff 8c 79 00 ?......?.....?y.
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
===================================================
Thank you.
Kyungwon
Kyungwon,
Register 0x13 should be 0x87 if your clock is 24.576Mhz.
are you using the EVM? if so how are you connecting the MCLK? note that by default MCLK is not connected to GPIO0 from J7 of the AC-MB. if you want this to happen R2 must be removed from the rear of the ADCx140EVM and R3 must be populated.
best regards,
-Steve Wilson
Hello Mr. Steve Wilson
No, I'm not using the EVM.
Actually, I'm using my own board now.
Yesterday, I realized I hadn't controlled IN_CH_EN/PWR_CFG properly.
So as of now, I'm able to see BCLK/FSYNC using oscilloscope.
But I'm still figuring out why I can't see any PDMCLK over IN1M_GPO1/IN2M_GPO2
In my board, IN1M_GPO1/IN2M_GPO2 is connected to each D-MIC's Clock.
Here is my i2c dump data.
root@euto-v9:~# i2cdump -f -y 7 0x4c
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 00 00 81 00 00 05 00 40 00 00 00 00 01 02 03 04 ..?..?.@....????
10: 05 06 07 87 42 42 10 10 04 20 02 08 00 00 02 41 ????BB??? ??..?A
20: 00 a0 40 40 00 00 00 00 00 00 00 45 00 00 00 00 .?@@.......E....
30: 00 00 00 ff 00 00 00 00 40 00 00 00 40 00 c9 80 ........@...@.??
40: 00 40 00 c9 80 00 00 00 c9 80 00 00 00 c9 80 00 .@.??...??...??.
50: 00 00 c9 80 00 00 00 c9 80 00 00 00 c9 80 00 00 ..??...??...??..
60: 00 c9 80 00 00 00 00 00 00 00 00 01 40 7b 00 00 .??........?@{..
70: e7 00 00 ff ff e0 ff e0 00 00 ff 00 ff 8c 93 00 ?....?.?.....??.
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
If you don't mind, could you let me know which thing I need to check?
Thank you.
Kyungwon