Other Parts Discussed in Thread: LM3914, TL084, LP5009, LP5024, TPIC6B595
I am working with cascading an LM3916 LED driver with an LM3915. The data sheet states the best practice is to use an op amp to increase the signal to the "first" IC. In my configuration, the 10V signal fed to the 3916 ("second" IC) with a V(REF) = 10V will cause LED 10 (+3 dB) to illuminate, indicating full scale. LED 10 of the "first" IC, an LM3915, is designed to illuminate at -30 dB. With 33 dB between LED 10 of each device, the data sheet implies that an op amp with A = 44.668 is needed.
With the audio signal attenuated to 10.0V under all circumstances, this signal is fed directly to the 3916. But fed through the op-amp with A = 44.7, this means the LM3915 pin 5 (SIG) will see 447 V. The data sheet states the LM3914/15/16 family can accept up to 35V max at pin 5 before damage occurs. Thus, following the data sheet means burning up the first LM39xx chip once volume levels increase.
What am I missing?