This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
When using the XSMT pin to mute the PCM5122 I have experienced that the output impedance is different when the DAC is muted and when it is not. I have tried to sweep the output impedance (using a BODE 100) and get an impedance reading of around 90ohm when the XSMT pin is low (muted) and <1 ohm when the XSMT pin is high (unmuted). What is the reason for this change in impedance?
I'm also using an LC filter in the output of the DAC - instead of the recommended RC filter. Will this be an issue for the DAC or create any instability?
Best regards
Tommy
Hi Tommy,
When the output is enabled, you are basically seeing an amplifier output (<1Ω makes sense). When you assert XSMT, the output amplifier is eventually powered down/disabled. In power down, the output is a bit higher impedance. When disabled, I believe the output is connected to ground through a high-ish impedance.
Thanks,
Paul
Hi Paul
Thank you for the explanation on the output impedance.
Do you have any experience regarding the LC output filter?
Regards
Tommy
Hi Tommy,
I have not seen too many questions about using an LC output filter. Do you have specific questions or schematic?
Thanks,
Paul