This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC6140EVM-PDK: Setup for 192ksps and 384ksps

Genius 12865 points
Part Number: ADC6140EVM-PDK
Other Parts Discussed in Thread: TLV320ADC6140

Hello Team,

what is required to use the TLV320ADC6140-EVM at a sample rate of 192ksps or even 384ksps (which are supported by the TLV320ADC6140), please?

Is this supported by PurePath GUI?

Thanks and Best Regards,

Hans

  • Hi Hans,

    PPC3 GUI can be used to configure the device registers. I am not sure if the USB Audio Interface to the PC supports 192/384 kHz. Our recommendation is to use  the external ASI interface of the ACMB (mother board).

    Best Regards.