This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
(Question)
When Mic input is not used on TLV320AIC3100, can it replace to TLV320DAC3100?
My customer thinks these are pin compatible(4/15PIN:NC) and registers are difference little bit.
Their understanding is correct? Can it replace to TLV320DAC3100?
Regards,
Tao_2199
Hello Tao,
DAC3100 is effectively the AIC3100 without the ADC paths. If the customer would like to add a mono ADC path to an existing TLV320DAC3100 design, then the TLV320AIC3100 is a great choice. They are largely 100% compatible.