Hi team,
Could you explain the exact behavior and purpose of the Bus Keeper function more in detail than which is described in SBAA415.pdf?
Does it hold the SDOUT to the last value (LSB=High or Low) to avoid floating the output?
I don't understand the example below.
"For example, the LSB of U2 could be set to transmit on the first half of the bit clock cycle,
while the MSB of U3 is driving without any offset. Moreover, selecting TX_KEEPER value of 0x2 or 0x3
adds robustness to the system by ensuring the LSB is latched properly by the host processor, since buskeepers
continue holding the bus with the last value driven."
regards,