This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Integrated audio CODEC plus speaker driver

Other Parts Discussed in Thread: TLV320AIC3120, TLV320AIC3110, TLV320AIC3111

Our requirements have changed and now we no longer need to meet Automotive temp grades.

We would like an integrated mono CODEC and speaker driver that can output 1 W into 8 Ohms (preferably from 3.3V supply) and also has a headset speaker driver. I see the TLV320AIC3120 but it doesn't have the 1W into 8 OHm capability. We also prefer the most power efficient speaker amplifier for obvious reasons. Do you have any recommendations?

Thanks,
Bruce

  • Hi Bruce,

    The TLV320AIC3111 and TLV320AIC3110 are the stereo 8Ω capable equivalent of the TLV320AIC3120 you referenced.  The TLV320AIC3110 has a fixed-function yet capable digital engine, while the TLV320AIC3120 is a fully configurable mini-DSP that uses PPS to develop desired processing flows.

    The AIC3111 and AIC3110 devices can drive 1.29W into 8Ω loads at 5.5V SPVDD supply voltages. 

  • Hi Collin,

    Thanks for the reply, but I think you didn't quite understand the question. We don't need stereo, only mono. And what we want is an integrated solution  that will drive an 8 Ohm speaker at 1 W with a 3.3V SPKRVDD. The TLV320AIC3120 can only drive 8 Ohms at <0.7 W for 3.3V SPKRVDD. Any other possibilities?

    Thanks,
    Bruce

  • Hi Bruce,

    The ones previously mentioned are our best fits.  You may find something with higher efficiency as a discrete ClassD, such as the TPA2010 or TPA2011, or something else in that portfolio.  Then you could use the TLV320AIC3109 (mono-ADC/mono-DAC) as the analog input to the Class-D. 

    I think you know this already which is why you're asking for high efficiency, but for other readers, with a +3.3V supply the maximum full-scale low-distortion output signal you could get with a differential driver is at most 6.6Vpp, or 2.3331Vrms, which into an 8Ω load yields about ~0.7W.

    Understood that the TLV320AIC3111 doesn't meet the +3.3V power output, but note that it is a mono-ADC/Stereo-DAC so there's only an extra DAC, not an extra ADC too if that helps.  

  • Ok, understood. Thanks for pointing that out. Looks like the TLV320AIC3120 is our best bet, then.