Hi,
I have a new design and attached are two codecs TLV320AIC3254.
The purpose of one of the AIC3254 codecs is to be able to sample and measure incoming frequencies above the plain audio spectrum and up to samplerate/2 (according to Nyquist).
Based on the AIC3254 datasheet it can have a samplerate of up to 192KHz.
I've managed to configure the AIC3254 in 32bit/192KHz (PRB_R13, PRB_P17)
I have two questions though,
1. if the AIC3254 can indeed listen any signal above 24KHz, or is there any anti-alias filter hardwired in the ADC path even if I do not place one?
2. is there any chart displaying the codec/ADC performance in higher than 24KHz frequency range?
Christos