Hello team,
I would like to ask some questions about the overshoot in the output pin of TAS2505.
1. What are the absolute maximum rating of outputs SPK-P / M pins?
My customers are worried that the overshoot and undershoot may be too big to break the device. At present, a voltage of about 7.4V is generated at the peak. Please refer to the attached file for the waveform.
2. I also found a statement in the E2E forum that device will not break at this level of overshoots, but is that true on this case too?
https://e2e.ti.com/support/audio/f/6/t/915514
3. Does the slow rise caused by the capacitor have an adverse effect on operation?
They are also planning to add a capacitor to suppress overshoot, and it seems that they confirmed the improvement of the waveform by attaching 22000pF to GND.
However, since the rise is slow (about 40nS), they are worried that this may have an adverse effect. Looking at the EVM, the SPK-P and SPK-M signal lines have a 4KΩ + 0.022uF filter, but if there is a recommended external circuit, please let me know.
I am looking forward to hearing from you.
Best Regards,
Ryotaro Fukui