This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5141: ZERO DATA DETECT IN PCM5141

Part Number: PCM5141

Hello sir,

May I ask whether the threshold of zero data can be adjusted for ZERO DATA DETECT function which when there is some noises below the threshold, the mute can be done as well?

Best regards,

wenting 

  • Hi Wenting,

    The zero-data detection is just a digital check of the DIN pin.  If there are enough samples where DIN = 0, then the device asserts the zero data detect.  Are you looking to implement a flag if the volume is set below a certain threshold?

    Thanks,

    Paul

  • Hello Paul,

    I've sent you a detail description through Email. Please help to have a look.

    Best regards,

    wenting