This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5624A: TAS5624 Power Output

Part Number: TAS5624A
Other Parts Discussed in Thread: TAS5624

hi, by referring to the THD vs Power Output graph inside the data sheet. Is it correct that the TAS5624 able to achieve 180W at 10%THD for a 4 ohm load?

  • Hi Mototw,

    Under the conditions specified in the datasheet, PVDD = 36V, same LC filter, etc, yes the TAS5624 should be able to achieve around 180W at 10% THD for a 4ohm load. You just need to make sure that you design the output traces to be able to handle these high current peaks, solid PVDD traces to minimize any drops in voltage, and proper selection of the output inductors that can handle the peak currents while also having a low DCR.

    Best Regards,

    Robert Clifton