Hello, I have a TAS5805MEVM connected to a 12V power supply and to my PC over USB. PurePath Console showing the board as offline and not showing the connect button. It is almost like the USB is not connected. The 3.3V LED is on, but the USB READY LED is off. I have S1 switched to XMOS, HS-EN, DVDD1 & DVDD2 jumpers are placed, J12-J14 are in BYPASS Position, and SCL and SDA jumpers are not placed. I believe this is the default jumpers configuration which we didn't change. What could cause this issue? Am I missing anything here?