This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi sir,
with ap test,adc5140 board and ap about MCLK BCLK FRAME CLK is ok,BUT no data in CODEC DOUT pin
i check the gui config output enable,and input ended single signal with CODEC IN1P is right
but dout have no data?i don't know why?
whether there some register to write???
no matter what ap with master or slave, CODEC inside IIS PIN,except DOUT no signal,others is ok,i test with oscilloscope.
where? I saw your suggestion before, after I followed it, the clock is normal, the sampling rate is normal, but there is no data.
I found another problem, that is, in the process of running the board, the loading was several times, and then it indicated that the valid I2C slave address could not be found
i check the reference register,
CH1_CFG0,ASI_OUT_EN, ti's write ok,i dont why the DOUT PIN no data,
i am sure the hw connections is ok, if the wrong config, the clk is not valid..
hi sir
we test the SNR with PPC3 sample 4CH single ended line input,the SNR about 98dB@1khz/20kbw with a-w
the same L/R SNR about 98dB
there is another case we test the high-level SNR??
Hi,
It sounds like you were able to resolve the majority of your issues and now have the correct data format. To measure datasheet performance you need to recreate the datasheet test conditions:
TA = 25°C, AVDD = 3.3 V, IOVDD = 3.3 V, fIN = 1-kHz sinusoidal signal, fS = 48 kHz, 32-bit audio data, BCLK = 256 × fS, TDM slave mode, PLL on (unless otherwise noted)
IN1 differential input selected and AC signal shorted to ground, DRE enabled (DRE_LVL = –36 dB, DRE_MAXGAIN = 24 dB), 2.5-kΩ input impedance selection.
It is best to measure the noise floor with the differential inputs shorted together and AC coupled to GND.
Best,
Zak
hi ,sir
with you advise,and the high perfermance level,the SNR test value also not achieve 120db
please check my report
This thread will be continued here: https://e2e.ti.com/support/audio/f/audio-forum/984289/adc5140evm-pdk-it-is-best-to-measure-the-noise-floor-with-the-differential-inputs-shorted-together-and-ac-coupled-to-gnd
Best,
Zak