Texas Instruments (TI) Audio support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search audio IC content or ask technical support questions on everything from audio amplifiers (op amps) and audio converters (Codecs and ADCs) to audio interface and media processors. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: TLV320DAC3203
Hi!
We are looking at cross reference requirements for the AK4377 for both commercial and automotive applications. What 2-channel DAC with integrated headphone driver can TI recommend as a replacement or upgrade?
Part Number: TLV320AIC3109-Q1
Hello,
I am looking through the data sheet of the TLV320AIC3109-Q1 and found the recommend power supply sequencing. Does this need to be followed? What could happen if it is not followed?
Regards, Aaron
Part Number: PCM1860 Other Parts Discussed in Thread: , PCM1861-Q1 , PCM1861 , PCM1808 , PCM1808-Q1 , TLV320ADC3140 , PCM1840 , TLV320ADC5140 , TLV320ADC6140
Hello,
We are looking for cross reference replacements for the AK5720 for both the commercial…
Part Number: TAS2563 I wish to use the Re value measured by TAS2563 externally. How can I get this value from the device?
where is Re located In the devices registers?
how do I read the value of Re from the device?
once the data has been read how…
Hello,
Configuring the PLL and clocks on the audio CODEC/ADC is a bit confusing to me. Is there an easy way to get or confirm the coefficients I need? I am using an input clock of 2.048MHz and wish to run at an Fs of 48kHz.
Thanks,
Aaron
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2562 Some applications have voltage regulators or voltage sources with base levels higher than 5.5V. In those cases it may be preferred to use direct connection from external voltage to PVDD instead…
Part Number: TLV320ADC5140 Hi. What are the power-up and power-down times for different sampling rates for the TLV320ADCx140 family? That family includes the following devices: TLV320ADC5140 , TLV320ADC6140 , TLV320ADC3140 .
Part Number: TAS2563 For TAS2563, under "Tuning and Audio Processing" of PPC3, what are those tuning tools used for?
Specifically:
Smart Amp Protection
Equalizer
Dynamic Range Compression
Dynamic Equalizer