This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have designed a board with the PCM1860 to operate in Master Mode. For testing I have been looking at the I2S signals DOUT, BCK, and LRCK. A problem that I am having is that the 7 LSB never vary, leading me to question what is happening. I also have a PCM1860EVM evaluation kit, and I am seeing the same results. The upper 17 bits vary with signal, but the 7 least signifcant bits are fixed at 0.
I have attached an image showing this (ignore the pink trace). Any thoughts on why the LSB would be fixed at 0, and not at least varying wildly at LSBs tend to do?
Thanks Justin. That makes sense; though I was expecting to see those bits vary even pseudo-randomly. So it is safe to say that those lower 7 bits will always remain low regardless of input signal?
The PCM1861 appears to be a direct drop-in replacement, is this right? Just wondering why it doesn't share the same datasheet as the PCM1860.