Part Number: TAS2563
Other Parts Discussed in Thread: TAS2562
Some applications have voltage regulators or voltage sources with base levels higher than 5.5V. In those cases it may be preferred to use direct connection from external voltage to PVDD instead of using internal boost embedded in TAS2563 and TAS2562.
- What are the required hardware modifications on the typical application diagram for external PVDD voltage?
- Is there any register that must be set for external PVDD voltage?
- Is there a specific power sequence required for external PVDD voltage?
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators