This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

a few minor issues in TI Clock Pro software v1.2

Hi,

First of all: good job on making a free tool for generating clock configurations without having to do all the calculations.

I am using TI Clock Pro to generate some configs for a CDCE919. The tool is great, but there are some minor issues:

-sometimes when using the wizard it will suggest using a different device with two PLLs even if my configuration is perfectly possible with a single PLL (it works when set manually)

-the bit viewer displays some register values (in hexadecimal) incorrectly, see my attached image --> register 23 has a value of 010, probably a bug in the decimal to hexadecimal library you are using

-this is more a minor complaint, but it is confusing when you use decimal values and hexadecimal values on the same page. The register number should also be in hexadecimal, because that is how they are numbered in the datasheet.