Other Parts Discussed in Thread: CODELOADER, USB2ANY, LMX2571EVM
When I connected up my LMX2571EVM per the instructions and started CodeLoader, the software detected it and said it needed to update the firmware on the USB2ANY. Then it choked halfway through the process. Now the USB2ANY doesn't come up as a recognized USB device; the green light comes up when I power it, but the software won't acknowledge it.
Regardless of whether I engage the paperclip reset or not, the Device Manager recognizes the USB2ANY as an HID device with VID 2047 PID 0200 REV 0104
I'm running Windows 10 and CodeLoader 4.20.2. Also, every time I start CodeLoader it tries to run my Microsoft Office installer, which I've got to say isn't even the slightest bit irritating.