Part Number: LMK03328
He Team,
Please advise me on a question bellow:
1. During the I2C access, PDN pin is set to Low, LMK03328 may pull SDA line to Low.
2. Once it happens, LMK03328 is keeping SDA low even though PDN returns to High.
3. The problem occurs when I2C access, other than LMK03328 on the same bus, is taken place.
I2C Access -----------XXXXXXXXXXX-------------------
___________
SDA XXX____________________
_________________ ____________
PDN |________|
Q1. Is this expected behavior?
Q2. If so, are there any way to recover from this situation?
Q3. Is there any workaround to be free from this trouble?
Is it the only solution that keeping PDN high during I2C access?
Q4. LMK03328 Datasheet recommends to toggle PDN to low for short
period time, after power up, do you need to hold I2C access during
this instance?
Mita