Part Number: LMX2572EVM
Other Parts Discussed in Thread: LMK61PD0A2, , USB2ANY, LMX2572
The Reference PRO Oscillator (LMK61PD0A2 ) is generating a proper oscillator signal for the LMX2572EVM (100MHz by default), but the LMX2572EVM is not generating any Output Signal (3GHz by Default).
I connected everything as it is described in the "LMX2572EVM Evaluation Instructions" (100 MHz LVPECL Clock, USB connected, 3.3V Supply, ribbon cable, RF etc.). The LEDs "MSP430 Supplied" and "LMK61xx Supplied" are on.
The Oscillator should be detected by the TICS Pro Software after connecting it via USB. TICS Pro indicates there is no Device Connected though (also when clicking on "USB Communication" -> "Interface" ->"USB2ANY"). After connecting the Oscillator to the computer, the Software should detect it and and ask for a Firmware update, which it doesn't.
In the Device Manager the MSP430 registers as HID with VID=2047 and PID=200. As VID and PID values are as described in “MSP430™ Flash Device Bootloader (BSL)” SLAU319S, page 7, I assume the MSP430 lost its FW and starts like a virgin device in boot mode.
Does anyone know that issue?
Regards
Michael