Part Number: LMX2491
Other Parts Discussed in Thread: LMX2594
Hi Guys
Our customer is taking a LMX2594 board in debugging, encountered the following two problems:
1. My requirement is that RFoutA outputs 5GHz, RFoutB outputs SYSREF, and SYSREF requires Repeat mode. just like below:
Input Clock: 50MHz please see below schematic:
But when we finished the configuration, the output frequency is always incorrect: we need 5GHz, but the output always 4.047GHz; please see below the configuration:
2. SYSREF has no output:
We input 3.3V, 1MHz square wave at SYSRefReq pin; And we input 3.3V 1kHz square wave at SYNC pin.
Result: RFoutA and RFoutB ,there is no output for both. please see our configuration:
could you review my problem? and your feedback are very appreciated.
Thanks
-Pengfei