Part Number: TPL5110
Hello.
I need to blink the LEDs every second. Is it possible to use the DRV output as a load for an LED?
Is the circuit below correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPL5110
Hello.
I need to blink the LEDs every second. Is it possible to use the DRV output as a load for an LED?
Is the circuit below correct?
Hi Ildar,
Load currents exceeding 1mA have not been characterized for this device. I recommend using a MOSFET or a buffer instead to drive the LED, and controlling the MOSFET/buffer state using the DRV pin.
Regards,