I'm looking for a programmable Frequency synthesizer similar to the TI Part No:LMX2541 with a FR out in the frequency range 1Gz to 2 GHz and Power output of min. 6dB with no compromise on the Phase noise.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do you have specific phase noise targets at some specific carrier frequencies? Or, where does LMX2541 compromise?
Can you elaborate more on programmable? For instance, what is the step size in the 1 GHz to 2 GHz range?
Perhaps you might consider the LMX2581? Max typ output power is 5 dBm @ 2.7 GHz. LMX2581 will cover 1 to 2 GHz.
73,
Timothy