Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fung
I have carefully confirmed that this spurs is not from the VCC.
I set the VCO frequency at 3300.002 MHz, the spurs appears at 3.3GHz, fpd = 100MHz, but I set the VCO frequency to 3301MHz, spurs also appeared at 3.3GHz, this is just a typical example, if I set the VCO frequency point 4001MHz, the spurs appears at 4GHz, the spurs is always in the integer multiples of fpd, so I guess is integer boundary spurs.
Hi Peng,
Right, in the above examples, the IBS will be 2kHz and 1MHz.
Since 2kHz is in-band, it is very difficult to resolve this problem. Reducing charge pump current may help a bit.
For 1MHz spurs, again reducing charge pump current may help. You can also use 4th order loop filter to increase filtering at 1MHz offset.