Part Number: LMK03318
Hi,
I have a question about the power supply sequence for the LMK03318.
As shown below, Is there any problem if there is a delay between power up of VDD_PLL, VDD_LDO, VDD_IN and VDD_DIG and power up of VDD_x ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK03318
Hi,
I have a question about the power supply sequence for the LMK03318.
As shown below, Is there any problem if there is a delay between power up of VDD_PLL, VDD_LDO, VDD_IN and VDD_DIG and power up of VDD_x ?
Hi,
There should be a delay between those supply groupings when operating under the split power rail condition. Please see 12.4.4 Powering Up From Split-Supply Rails from the datasheet.
1.8 V supply should be applied once the 3.3 V supply reaches 2.72 V.
PDN should be asserted once 1.8 V supply reaches 1.71 V

Regards,
Jennifer