Part Number: LMK1C1102
What is the output current drive capability of the LMK1C1102 running with a VDD = 1.8V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK1C1102
What is the output current drive capability of the LMK1C1102 running with a VDD = 1.8V?
Hi Jason,
Based on the load condition defined below in the datasheet you can have a drive current of about 16 mA at 1.8 V. This is based on the output driver impedance of 60 ohm mentioned in the datasheet.
driver current = VDD / output impedance + load impedance = 1.8 V / 60 ohm + 50 ohm = 16.3 mA

Best,
Asim