This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVP1208: Unused input to create an "output enable" pin

Part Number: CDCLVP1208


Hello,

I am interested in using the CDCLVP1208 but my design requires an output enable pin. Since I only have one input, I was thinking I could connect my input clock signal to IN1 and leave IN0 floating. I would put a pulldown resistor on IN_SEL so the input mux defaults to IN0. Then, IN_SEL would effectively work as an active high output enable pin because if I put a 1 on IN_SEL, it will connect IN1 to the outputs. When IN_SEL is driven to 0, there would be no output from the device.

Would the setup I described work to effectively give me an output enable pin for this device? Do you foresee any issues with this setup?

Thank you!

Best regards,

Zach Kimble