Other Parts Discussed in Thread: LMK5C33216, LMK05028, LMK5C33216A
Hello,
I bought the LMK5C33216 EVM to test with1-PPS inputs as the reference clock.
I would connect a PPS to IN0 (1Hz) and I would like to have the following ouputs:
- A PPS (out 0) in LVDS,
- 38.88 MHz (out 1) synchronised to the input PPS and phase aligned with PPS out0,
I have tested with LMK05028 without success.
1) Do you have .tcs file for testing with LMK5C33216 EVM ?
2) I can use a PPS as input a CMOS 1V8 (0V /1V8) or a CMOS 3V3 (0V /3V3)?
Thank you,
Best regards,
Patrice