This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: New to LMX2595 EVM board

Part Number: LMX2595

Hi, 

I am writing to request guidance on setting up the LMX2595 EVM board. I am new to working with this board. My primary goal is to just achieve a 10GHz RF output signal without delving deeply into the technical aspects of PLL configuration. I've already installed the TICS Pro software and made the necessary hardware connections (Pics attached). However, I have been experiencing challenges in achieving the desired 10GHz RF output. At times, the default configuration produces a 7GHz signal, while at other times the signal disappears entirely.

I would be grateful if someone could help me with clear and simple steps to achieve a 10GHz RF output signal using the LMX2595 EVM, Reference Pro boards, and TICS Pro configuration.