Hello,
I am trying to determine if I can operate this component in the desired mode (FSK triggered by digital pin). Nominal Frequency 2200MHz, modulate at 10MHz, with a frequency deviation of 7MHz (0.7 Index). I would need a loop bandwidth approximately 20MHz (roughly two times the modulation rate), is this advisable with this part? On PLLatinum sim, it looks like a I can get >50 degrees phase margin,
Kind Regards,
Joe