This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571: LMX2571 1Ghz Frequency out from 10MHz reference clk but spur is insane

Part Number: LMX2571

Tool/software:

I am trying LMX2571 aliexpress board and I got succeed on board osc(100MHz)  make 1.0GHz out

So after than I try external refernce clk(10MHz)

But it show +-2.45KHz offset peaks(-33db from center) added a lot on my spectrum plot

What I got changed things are

1) Fosc 100MHz -> 10MHz

2) MULT_WAIT(2000 -> 200)

And nothing.. I checked reference clk end of the osc_in...

so I checked signal min was -300mv so i got connect DC to up minimum to 200mV

But result is same

What should i check more..? 

I think loop filter is ok because same Fpd setting was operated well

this is schematic about external reference clk input