This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334-Q1: V differential peak to peak min and max output amplitudes

Part Number: LMK00334-Q1

Tool/software:

Hi, Can you tell me what the V differential peak to peak min and max output amplitudes is for the LMK00334-Q1? I have a unique application and need to know the worse case V differential peak to peak min and max output.

  • Al,

    We can calculate this based on the single ended absolute high/low voltages.  MAX VOH = 920mV and MIN VOL = -150mV makes the absolute max swing 1.07V which differential would be 2.14V

    With MIN VOH = 520mV and MAX VOL being 150mV that means the absolute min swing is 370mV which differential would be 740mV. 

    Although the max/min combinations that create a worst case spec are very unlikely and nominally the chip will have a differential swing of 1.62V.

    Regards,

    Will