Other Parts Discussed in Thread: LMX2492
Tool/software:
Hi all
I use LMX2492 in my FMCW radar , i find that if i set LMX2492 to CW ,the spectrum after ADC sampled is clean . it just has some sub fraction spurs,the level of the sub fraction is a little high if i do not open the dither.
but when i set LMX2492 to Ramp, i can always see nearly 200kHz spur near the spectrum of IF
i check the power , the clock and my configuration , i think they are correct.
So i need check with TI about that Does this chip has some problems just like my describection. because if you set this chip to Ramp, the FRAC_DEN will be set to 2^24, this is not the same as CW.
Could you give me some suggestion?
FMCW
CW