This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: What will IncludedDivide be if channel divider is 2?

Part Number: LMX2594

Tool/software:

Hi,

I use the two LMX2495 in my board, and want to sync the output clock(3932.16MHz) between them. As below figure.1 shown, my configuration is that Fosc =122.88MHz and Fout = 3932.16MHz。

 It conform to SYNC Category 1, so I set VCO_PHASE_SYNC=1. I find channel divider=2 but IncludedDivide=4 in the figure.3. My understanding is that IncludedDivide come from channel divider, so IncludedDivide must be less than channel divider. But now,  IncludedDivide are bigger than channel divider. My questions are:

1. Whether will this configuration work normally? 

2. N Divider(16) will turn red that the tip show that the minimum N divide for any modulator order is 28 , but I don't use MASH order function. Whether will this red warning impact my configuration?

Figure.1

Figure.2

Figure.3

Figure.4

Thanks in advance!

Best regards!

Jason